AXIS#.MT.TYPE

Description

This keyword sets the motion task control word with the motion task type information.

It takes the following values:

0 Absolute
1 Relative To Command Position
2 Relative to previous target position
3 Relative to external position
4 Relative to feedback position

Examples

Usage

This keyword is used to set what you would otherwise have set with AXIS#.MT.CNTL.

Code

MT.TYPE 0 2 Will configure Motion Task 0 as a move relative to previous target position.

Context

See AXIS#.MT.CNTL for more information on the argument semantics.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only Array
Units N/A
Range 0 to 4
Default Value 0
Data Type Integer
See Also  
Start Version  

Stored in Non-Volatile Memory

No

Variants Supported

Supported on all drives.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MT.TYPE 0

50e1h

01h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 1

50e1h

02h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 2

50e1h

03h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 3

50e1h

04h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 4

50e1h

05h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 5

50e1h

06h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 6

50e1h

07h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 7

50e1h

08h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 8

50e1h

09h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 9

50e1h

0ah

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 10

50e1h

0bh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 11

50e1h

0ch

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 12

50e1h

0dh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 13

50e1h

0eh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 14

50e1h

0fh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 15

50e1h

10h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 16

50e1h

11h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 17

50e1h

12h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 18

50e1h

13h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 19

50e1h

14h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 20

50e1h

15h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 21

50e1h

16h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 22

50e1h

17h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 23

50e1h

18h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 24

50e1h

19h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 25

50e1h

1ah

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 26

50e1h

1bh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 27

50e1h

1ch

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 28

50e1h

1dh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 29

50e1h

1eh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 30

50e1h

1fh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TYPE 31

50e1h

20h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6318

1

6318 (0x18ae)

AXIS1.MT.TYPE

Unsigned8[32]

Read/Write

Yes

71854

2

6318 (0x18ae)

AXIS2.MT.TYPE

Unsigned8[32]

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.MT.TYPE

6318

Unsigned8[32]

Read/Write

-